AXIS#.HOME.DIST

Description

After the axis has completed the sequence to find the home position, AXIS#.HOME.DIST allows an additional movement, relative to the new home position. This extra movement allows the axis to move away from the found home position by this distance. A value of 0 will prevent any movement and leave the axis at the found home position.

This additional movement uses the homing acceleration, deceleration, and velocity.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

This content is not applicable to KAS.

Type

Read/Write

Units

Depends on AXIS#.UNIT.PROTARY or AXIS#.UNIT.ACCLINEAR

Rotary: counts, rad, deg, Custom Units, 16-bit counts

Range

Depends on units. See Position Range for details.

Default Value

0

Data Type

Float

See Also

AXIS#.HOME.ACC, AXIS#.HOME.DEC, AXIS#.HOME.V
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
AXIS1.HOME.DIST

5008h

09h

Signed32

Position

-

Read/Write

No

AXIS2.HOME.DIST

5108h

09h

Signed32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.DIST

6104

17D8

Signed32

Read/Write

Position

AXIS2.HOME.DIST

71640

117D

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.DIST

6104

Signed32

Read/Write

Position

Related Topics

Homing